Task: Free running conversion on ADC channel 0. Use of conversion complete
interrupt.
In this program, the ADC module is initialized and runs in free running mode
in the adc_free_run_mode()
routine. As the ADC conversion complete
interrupt is enabled, the Interrupt Service Routine for this interrupt will be triggered
as soon as a conversion is completed. In Free Running mode, a new conversion will be
started immediately after a conversion completes. The ADSC bit remains high during a
conversion. The time between two consecutive ADC samples depends on the ADC conversion
time.
- 1.Select ADC channel 0 by writing the
Analog Channel Selection bit group in the ADC Multiplexer Selection register
(ADMUX.MUX) to '0b0000'.
- 2.Select internal reference to 1.1V by
writing the Reference Selection bit in ADMUX (ADMUX.REFS0) to '0'.
- 3.Enable the ADC module by writing the
ADC Enable bit in the ADC Control and Status A register (ADCSRA.ADEN) to '1'.
- 4.Select system clock prescaling to 16
by writing the ADC Prescaler Select bit group in ADCSRA (ADCSRA.ADPS) to
'0b100'.
- 5.Enable auto triggering by writing the
ADC Auto Trigger Enable bit in ADCSRA (ADCSRA.ADATE) to '1'.
- 6.Enable free running mode by writing
the ADC Auto Trigger Source bit group in the ADC Control and Status B register
(ADCSRB.ADTS) to '0b000'.
- 7.Start the first conversion by writing
the ADC Start Conversion bit in ADCSRA (ADCSRA.ADSC) to '1'.
- 8.Optionally, wait for the Interrupt
Flag bit in the ADCSRA register to be set, indicating that a new conversion is
finished.
- 9.After the conversion is over (ADIF
bit becomes high) the CPU executes the ADC interrupt service routine where the ADC
data register pair (ADCL/ADCH) is read to get the 10-bit ADC result.
Note: It is not necessary to wait for the
interrupt flag when using free-running mode. However, to make sure of a fresh
conversion, wait for the flag to set, clear it and then read the result.
Test Steps
Refer to Test Steps.