The steps to start exploring the
Xplained Pro platform are the following:
Note: For more details, refer to the
WLR089 Xplained Pro Evaluation Kit (EV23M25A) Quick Start Guide(
DS00003487A).
When the WLR089 Xplained Pro Evaluation kit is connected
to the host PC for the first time, the operating system installs the driver software
automatically. This driver supports 32-bit and 64-bit versions of Microsoft®
Windows® XP, Windows Vista®, Windows 7,
Windows 8, Windows 10 and Windows Server 2012.
Observe the following changes after powering on the
WLR089 Xplained Pro Evaluation board:
- The green power LED D400
turns on.
- Atmel Studio automatically
detects the connected Xplained Pro and extension board(s).
- In Atmel Studio, the landing
page of the kit presents an option to launch the associated ASF.
Notes:
- Ensure that only
the on-board embedded debugger is used for debugging, not
another debugger like Atmel-ICE or SAM-ICE.
- For more details, refer to the SAM R34 MLS Getting Started
Guide (DS50002812).