Operating at Other Voltages

The WLR089 Xplained Pro Evaluation board operates at 3.3V by default, but it is also possible to run the board at lower voltages from an external supply. The EDBG is designed to run from a 3.3V supply and will not work on other voltages; therefore, all connections from the EDBG and from the on-board 3.3V regulator to the WLR089U0 module must be removed.

To completely disconnect the EDBG and the on-board power supply from the WLR089U0 module, perform the following steps:

Info: Operating the WLR089U0 module at voltages other than 3.3V requires physical modifications on the kit using a soldering iron and an external debugger for programming the WLR089U0 module. The on-board current measurement only works at 3.3V. The on-board LED is selected for 3.3V operation; the LED brightness at 1.8V operation is dull. To increase the emitted light level, the value of the series resistor can be lowered. EDBG functionality can be restored by re-soldering the removed components.
CAUTION: The voltage supplied through the power header is applied directly to the WLR089U0 module and the extension headers. Applying a voltage greater than 3.5V may damage the board permanently.
Figure 1. WLR089 Xplained Pro Evaluation kit Current Measurement Headers