On the WLR089 Xplained Pro, the MCU and
the MCU peripherals (for example, extensions) are powered by their own regulator, as
shown in the following figure. All other parts of the board, mainly the embedded
debugger and accompanying Xplained Pro Analog Module (XAM), are powered from a separate
regulator. The current to the MCU and peripherals can be measured by connecting them to
the XAM output through jumper settings.
Figure 1. WLR089 XAM Implementation
Block Diagram
XAM can be used in four configurations on the
WLR089 Xplained Pro Evaluation board:
- 1.No current measurement or
external MCU current measurement: The XAM is bypassed and thus the
module and peripherals are supplied directly by the regulator. Set both jumpers
in the "BYPASS" position. In this configuration, it is also possible to connect
external measurement tools on the module Xplained Pro power measurement header
to measure the module current directly instead of using the XAM.
- 2.Module current
measurement: The XAM measures only the module current while the peripherals
are supplied directly by the regulator. For this configuration, place the jumper
for "I/O" (peripherals) into the "BYPASS" position and the jumper for "MCU" into
the "MEASURE" position.
- 3.Peripherals measurement:
The XAM measures only the peripherals current while the module is directly
supplied by the regulator. For this configuration, place the jumper for "MCU"
into the "BYPASS" position and the "I/O" jumper into the "MEASURE"
position.
- 4.Module and peripherals
measurement: In this configuration, both the module and peripherals are
measured by the XAM. Place both jumpers on "I/O" and "MCU" headers in the
"MEASURE" position.