To connect the board, perform the following steps:
- 1.Connect one of the USB cables from the PC to the USB connector on the board.
- 2.Connect LCPS to the PC with a USB cable.
- 3.Connect LCPS to the programming header on the board.
- 4.Connect the 5V power supply to the board.