The on-board debugger and level shifters can be completely disconnected from the AVR128DB48.
The block diagram below shows all connections between the debugger and the
AVR128DB48. The rounded boxes represent connections
to the board edge. The signal names shown are also printed in silkscreen on the bottom
side of the board.
To disconnect the debugger, cut the straps shown in Figure 2.
Attention: Cutting the GPIO straps to the on-board debugger will disable the
virtual serial port, programming, debugging, and data streaming. Cutting the power
supply strap will disconnect the on-board power supply.
Tip: Any connection that is cut
can be reconnected using solder. Alternatively, a 0Ω 0402 resistor can be
mounted.
Tip: When the debugger is
disconnected, an external debugger can be connected to holes shown in
Figure 2. Details about connecting an external debugger are
described in
Connecting External Debuggers.
Figure 1. On-Board Debugger Connections
Block Diagram
Figure 2. On-Board Debugger Connection Cut Straps