Control A
Bit7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
RUNSTDBY | LOWLAT | ENABLE | |||||
AccessR/W | R/W | R/W | |||||
Reset0 | 0 | 0 |
Run in Standby
This bit controls whether the ADC will run in Standby sleep mode or not.
Value | Description |
---|---|
0 | The ADC will not run in Standby sleep mode. An ongoing conversion will finish before the ADC enters sleep mode. |
1 | The ADC will run in Standby sleep mode. The main clock will be requested when the ADC is triggered to perform a conversion. |
Low Latency
This bit controls whether the analog modules required by the ADC are enabled continuously or only when needed.
Value | Description |
---|---|
0 | The ADC enables the required analog modules only when starting a conversion. This reduces the overall power consumption of the ADC and increases the initialization time when starting an ADC conversion. |
1 | The
analog modules stay enabled when selected as input to the ADC. Using this
setting will minimize the initialization time of the ADC. Note: LOWLAT does not keep the
clock source enabled when the ADC is not converting, so a clock startup
delay may be experienced even though LOWLAT is set. To avoid such a
delay, make sure that the clock source is always
enabled.
|
ADC Enable
This bit controls whether the ADC is enabled or not.
Value | Description |
---|---|
0 | The ADC is disabled |
1 | The ADC is enabled |