The figure below shows the timing diagram for the ADC when running in Burst Accumulation mode without using the PGA.
1
’ in
the Control A (ADCn.CTRLA) register, the analog modules in the ADC will not turn OFF at
the end of the conversion, eliminating the initialization time when triggering the
following conversion.The number of samples to accumulate is set by the Sample Number (SAMPNUM) bit field in the Control F (ADCn.CTRLF) register.
The total conversion time (tconv) for a Burst Accumulation, in μs, is calculated by:
The Burst Accumulation conversion rate (fconv) is calculated by: