It is possible to use the UPDI to get an accurate measurement of the system clock
frequency by utilizing the UPDI event connected to TCB with Input Capture capabilities.
A recommended setup flow for this feature is given by the following steps:
- Set up TCBn.CTRLB with setting
CNTMODE =
0x3
, Input Capture Frequency Measurement mode
- Write CAPTEI =
1
in TCBn.EVCTRL to enable Event Interrupt. Keep EDGE = 0
in
TCBn.EVCTRL
- Configure the Event System to
route the UPDI SYNCH event (generator) to the TCB (user)
- For the SYNCH character used to
generate the UPDI events, it is recommended to use a slow baud rate in the range
of 10-50 kbps to get a more accurate measurement of the value captured by the
timer between each UPDI event. One particular thing is that if the capture is
set up to trigger an interrupt, the first captured value must be ignored. The
second captured value based on the input event must be used for the measurement.
See Figure 1 for an example using 10 kbps
UPDI SYNCH character pulses, giving a capture window of 200 µs for the
timer.
- It is possible to read out the
captured value directly after the SYNCH character by reading the TCBn.CCMP
register, or the value can be written to memory by the CPU once the capture is
done. For more details, refer to the TCB - 16-bit Timer/Counter Type B
section.
Figure 1. UPDI System Clock Measurement
Events