Some of the analog modules in the ADC are disabled between conversions and require time to initialize before a conversion starts. Only the modules used by the current ADC configuration are enabled, and as the initializations run in parallel, the limiting factor is the module with the slowest initialization time. The following table shows the different initialization times needed by the analog modules.
Analog Module | Initialization Time |
---|---|
ADC | 10 µs(1) |
PGA | 20 µs |
Settling of internal references | 60 µs |
Internal Tempsense input | 35 µs |
Internal DAC input | 35 µs |
Example: Selecting Tempsense as input and using VDD as the reference will give a 35 µs initialization time. Using the Tempsense with the 1.024V internal reference will result in a 60 µs initialization time.
The ADC can be put in Low-Latency mode by writing a ‘1
’ to the LOWLAT
bit in the Control A (ADCn.CTRLA) register. This will keep the configured modules
continuously enabled, effectively removing all initialization time at the start of a
conversion. The initialization time is still needed when enabling the ADC for the first
time, and if reconfiguring the ADC to use an input or reference that requires
initialization, as shown in the table above. The ADC Busy (ADCBUSY) bit in the Status
(ADCn.STATUS) register can be used to check if initialization is ongoing.
The sampling period of the input to the ADC is configured through the Sample Duration (SAMPDUR) bit field in the Control E (ADCn.CTRLE) register as (SAMPDUR + ½) CLK_ADC cycles. The input signal characteristics affect how long the sampling period has to be.
When the PGA is used, it is sampling continuously and will only be in the Hold state when the ADC is sampling the PGA. This ADC PGA Sample Duration (ADCPGASAMPDUR) depends on fCLK_ADC and is configured in the PGA Control (ADCn.PGACTRL) register. SAMPDUR will still configure the minimum sampling period of the input to the PGA as (SAMPDUR + 1) CLK_ADC cycles. In Burst mode, SAMPDUR must be ≥12, limited by the length of the Conversion state.
The Series and Burst Accumulation modes can be used for oversampling to achieve up to 5 bit higher resolution, given suitable input signal and sampling frequency. Increasing the resolution by n bits can be achieved by accumulating 4n samples and dividing the accumulated result by 2n. The Sample Accumulation Number (SAMPNUM) bit field in the Control F (ADCn.CTRLF) register can be configured for up to 45 = 1024 samples, resulting in up to 17-bit resolution.
The two tables below show the calculated conversion rates (fconv) for a subset of the possible combinations of fCLK_ADC and sample durations. For more details, see the relevant timing diagrams on the following pages.
SAMPDUR | PGA | fconv(1) Single 8-bit [sps] | fconv(1) Single 12-bit [sps] | fconv Burst Accumulation [sps] |
---|---|---|---|---|
2 | OFF | 384615 | 294118 | 312500 |
12 | OFF | 217391 | 185185 | 192308 |
48 | OFF | 84746 | 79365 | 80645 |
255 | OFF | 18797 | 18519 | 18587 |
2 | ON | 149254 | 133333 | N/A |
12 | ON | 114943 | 105263 | 147059 |
48 | ON | 62893 | 59880 | 71429 |
255 | ON | 17452 | 17212 | 18051 |
SAMPDUR | PGA | fconv(1) Single 8-bit [sps] | fconv(1) Single 12-bit [sps] | fconv Burst Accumulation [sps] |
---|---|---|---|---|
2 | OFF | 25641 | 19608 | 20833 |
12 | OFF | 14493 | 12346 | 12821 |
48 | OFF | 5650 | 5291 | 5376 |
255 | OFF | 1253 | 1235 | 1239 |
2 | ON | 17094 | 14184 | N/A |
12 | ON | 11299 | 9950 | 16667 |
48 | ON | 5089 | 4796 | 5952 |
255 | ON | 1223 | 1206 | 1267 |
1
’ in the Control F
(ADCn.CTRLF) register; a new conversion will be started immediately after the
results are available in the ADC.