The figure below shows the timing diagram for the ADC when running in Single 8- or 12-bit mode without using the PGA.
1
’ in
the Control A (ADCn.CTRLA) register, the analog modules in the ADC will not turn OFF at
the end of the conversion, eliminating the initialization time when triggering the
following conversion.The total conversion time (tconv) for a single result, in μs, is calculated by:
A new conversion starts immediately after a result is
available in the Result (ADCn.RESULT) register if the Free-Running (FREERUN) bit is set to
‘1
’ in the Control F (ADCn.CTRLF) register. The Free-Running conversion
rate (fconv) is calculated by: