The inputs can be individually:
The output from a sequencer can be used as an input source for the two LUTs it is connected to.
When selected (INSELy = FEEDBACK in LUTnCTRLx), the sequencer (SEQ) output is used as input for the corresponding LUTs.
When selecting the LINK input option, the next LUT’s direct output is used as LUT input. In general, LUT[n+1] is linked to the input of LUT[n]. LUT0 is linked to the input of the last LUT.
Events from the Event System can be used as inputs to the LUTs by writing to the INSELn bit groups in the LUT n Control B and C registers.
When selecting the IO option, the LUT input will be connected to its corresponding I/O pin. Refer to the I/O Multiplexing and Considerations section in the data sheet for more details about where the LUTn-INy pins are located.
The different peripherals on the three input lines of each LUT are selected by writing to the Input Select (INSEL) bits in the LUT Control (LUTnCTRLB and LUTnCTRLC) registers.