An event, as used in this document, is an indication that a change of state within a peripheral has occurred. A peripheral capable of generating events is called an event generator. One event generator may be able to generate events on several changes within the peripheral. Each of these is an individual event source. As an example, a timer/counter module is an event generator with several event sources, since it can generate events on overflow and compare/capture.