Important: Launching MCC v3.95 or
earlier will automatically install an obsolete deprecated version of the AVR-IoT WG
library. To avoid using this outdated library and its components, always check that you
are loading the
AVR-IoT AWS Sensor Node Library and not
the "AVR-IoT WG Sensor Node" Library. The correct library will also have a blue question
mark beside its name as shown below. The correct component libraries used by the module
will be under
Libraries in Device Resources panel.
- CrypthoAuthLib – The Crypto
Authentication Library (CryptoAuthLib) shows the settings needed to configure the
on-board ECC608 chip that provides the security features of the AVR-IoT WA board to work. It also indicates the communication settings
between the ECC608 chip and the embedded microcontroller on-board, as shown in CryptoAuthLib MCC.
- WINC – Under the WINC library, the
user can configure the default SSID, password, authentication type, and inclusion of
IPSocket for the network to which the board will be connected, as seen in WINC MCC.
- Message Queuing Telemetry Transport
(MQTT) – MQTT is used as a messaging protocol which operates on top of a TCP/UDP
connection to transporting data between client and broker over the Cloud. In MCC,
the user can change their MQTT host and connection time-out duration, as shown
inMQTT MCC for desired application configuration).
Figure 1. CryptoAuthLib MCC
Figure 2. WINC MCC
Figure 3. MQTT MCC