Getting started with the PIC16F152 family of 8-bit microcontrollers requires attention to a minimal set of device pin connections before proceeding with development.
The following pins must always be connected:
These pins must also be connected if they are being used in the end application:
Additionally, the following may be required:
The minimum recommended connections are shown in the figure below.