TMR2 - Timer2 Module

The Timer2 module is an 8-bit timer that incorporates the following features:

See figure below for a block diagram of Timer2.

Important: References to module Timer2 apply to all the even numbered timers on this device (Timer2, Timer4, etc.).
Figure 1. Timer2 with Hardware Limit Timer (HLT) Block Diagram
Notes:
  1. 1.Signal to the CCP peripheral for PWM pulse trigger in PWM mode.
  2. 2.See RSEL for external Reset sources.
  3. 3.See CS for clock source selections.