If the boot read lock is enabled,
the range CRC cannot end on the last address of the application section. If the
application table read lock is enabled, the range CRC cannot end on the last address
before the application table.
Workaround
Ensure that the end address used in Range CRC does not end
at the last address before a section with read lock is enabled. Instead, use the
dedicated CRC commands for complete application sections.
Affected Silicon Revisions
ATxmega16A4U |
Rev. A - D |
Rev. E |
* |
X |
ATxmega32A4U |
Rev. A - D |
Rev. E |
* |
X |
ATxmega64A4U |
Rev. A-B |
Rev. C |
Rev. D |
* |
X |
X |