Reading the memory arrays is handled using the
LD*/LPM(1)
instructions.
The erase of the whole Flash (
CHER) or the
EEPROM (
EECHER) is started by writing commands to the
NVMCTRL.CTRLA register. The other write/erase operations are just enabled by writing
commands to the NVMCTRL.CTRLA register and must be followed by writes using
ST*/
SPM(1) instructions to the memory
arrays.
Note:
- 1.LPM/SPM cannot be used for
EEPROM.
To write a command in the NVMCTRL.CTRLA register, the following sequence needs to be
executed:
- 1.Confirm that any previous operation is completed by reading the Busy (EEBUSY and
FBUSY) flags in the NVMCTRL.STATUS register.
- 2.Write the appropriate key to the Configuration Change Protection (CPU.CCP) register
to unlock the NVM Control A (NVMCTRL.CTRLA) register.
- 3.Write the desired command value to the CMD bit field in the Control A
(NVMCTRL.CTRLA) register within the next four instructions.
The following steps are required to perform a write/erase operation in the NVM:
- 1.Confirm that any previous operation
is completed by reading the Busy (EEBUSY and FBUSY) flags in the NVMCTRL.STATUS
register.
- 2.Optional: If accessing the Flash in
the CPU data space, map the corresponding 32 KB Flash section into the data space by
writing the FLMAP bit field in the NVMCTRL.CTRLB register.
- 3.Write the desired command value to
the NVMCTRL.CTRLA register as described before.
- 4.Write to the correct address in the
data space/code space using the ST*/SPM
instructions.
- 5.Optional: If multiple write
operations are required, go to step 4.
- 6.Write a NOOP or
NOCMD command to the NVMCTRL.CTRLA register to clear the
current command.