The compare channels can be used for waveform generation on the corresponding port pins. The following requirements must be met to make the waveform visible on the connected port pin:
1
in TCAn.CTRLB), which will override the output
value for the corresponding pin. An alternative pin can be selected by configuring the
Port Multiplexer (PORTMUX). Refer to the PORTMUX - Port Multiplexer section for
details.