The following steps are recommended to initialize ADC operation:
- 1.Configure the ADC voltage reference
in the Voltage Reference (VREF) peripheral.
- 2.Optional: Select between Single-Ended
or Differential mode by writing to the Conversion Mode (CONVMODE) bit in the Control
A (ADCn.CTRLA) register.
- 3.Configure the resolution by writing
to the Resolution Selection (RESSEL) bit field in the ADCn.CTRLA register.
- 4.Optional: Configure to left adjust by
writing a ‘
1
’ to the Left Adjust Result (LEFTADJ) bit in the
ADCn.CTRLA register.
- 5.Optional: Select the Free-Running mode by writing a ‘
1
’ to the
Free-Running (FREERUN) bit in the ADCn.CTRLA register.
- 6.Optional: Configure the number of
samples to be accumulated per conversion by writing to the Sample Accumulation Number
Select (SAMPNUM) bit field in the Control B (ADCn.CTRLB) register.
- 7.Configure the ADC clock (CLK_ADC) by
writing to the Prescaler (PRESC) bit field in the Control C (ADCn.CTRLC)
register.
- 8.Select the positive ADC input by
writing to the MUXPOS bit field in the ADCn.MUXPOS register.
- 9.Optional: Select the negative ADC
input by writing to the MUXNEG bit field in the ADCn.MUXNEG register.
- 10.Optional: Enable Start Event input by
writing a ‘
1
’ to the Start Event Input (STARTEI) bit in the Event
Control (ADCn.EVCTRL) register, and configure the Event System accordingly.
- 11.Enable the ADC by writing a
‘
1
’ to the ADC Enable (ENABLE) bit in the ADCn.CTRLA
register.
Following these steps will initialize the ADC for basic measurements.
For details about the start-up time of the VREF peripheral, refer to the
Electrical Characteristics section.
The ADC does not consume power when the ENABLE bit is ‘0
’. The
ADC generates a 10- or 12-bit result which can be read from the Result (ADCn.RES)
register.
Notes: Changing the following registers during a
conversion will give unpredictable results:
- In ADCn.CTRLA:
- Conversion Mode (CONVMODE)
bit
- Left Adjust Result (LEFTADJ)
bit
- Resolution Selection (RESSEL)
bit field
- In ADCn.CTRLB:
- Sample Accumulation Number
Select (SAMPNUM) bit field
- In ADCn.CTRLC:
- Prescaler (PRESC) bit
field