The Virtual PORT registers map the most frequently used regular PORT registers into the I/O
Register space with single-cycle bit access.
Access to the Virtual
PORT registers has the same outcome as access to the ordinary registers allowing for
memory-specific instructions, such as bit manipulation instructions, which cannot be
used in the extended I/O Register space where the regular PORT registers reside.
The following table shows the mapping between the
PORT and VPORT registers.
Table 1. Virtual Port Mapping
Regular PORT Register |
Mapped to Virtual PORT Register |
PORTx.DIR |
VPORTx.DIR |
PORTx.OUT |
VPORTx.OUT |
PORTx.IN |
VPORTx.IN |
PORTx.INTFLAGS |
VPORTx.INTFLAGS |
Note: Avoid accessing the mapped VPORT register using the single-cycle I/O instructions
immediately after accessing the regular PORT register. This may cause a memory collision
since the single-cycle I/O access to VPORT is faster than the regular PORT register access.