rtcountStruct Struct
Members
- rtcountcallback_ptr_t rtcountStruct::callbackPtr
- This is a pointer to the callback handler
- void * rtcountStruct::payload
- This is a value that can be passed on to the callback
- struct rtcountStruct *volatile rtcountStruct::next
- This is a pointer to the next timer on the queue
- uint32_t rtcountStruct::absoluteTime
- This is the number of ticks the timer will count down