This function checks the list of expired timers and calls the first one in the list if the list is not empty. It also reschedules the timer if the callback returned a value greater than 0.It is recommended this is called from the main superloop (while(1)) in your code but by design this can also be called from the timer ISR. If you wish callbacks to happen from the ISR context you can call this as the last action in timeout_isr instead.
void timeout_callNextCallback( void )
Type: void