This handler executes a repeating, periodic timer that uses a payload argument.
static uint32_t periodic_handler_payload( void * payload )
Type: void *
- any value that needs to be passed onto the handler.
Type: uint32_t