oneshot_handler
This timeout callback handler returns 0, does not reschedule the timer, so will execute only once.
periodic_handler
This timeout callback handler continuously reschedules a periodic timer to timeout with the number of ticks it returns.
periodic_handler_payload
This handler executes a repeating, periodic timer that uses a payload argument.
counter_handler
This handler executes a repeating timer that counts the ticks while an event is going on.
Timeout_example_create_sched_oneshot
Call this function to run a 1000-tick timer once. The timer will not be rescheduled in the associated callback function.
Timeout_example_create_sched_periodic
Call this function to run a 1000-tick timer continuously. The callback function reschedules the timer continuously.