On Windows machines, the CDC will enumerate as Curiosity Virtual COM Port and appear in the Ports section of the Windows Device Manager. The COM port number can also be found there.
On Linux machines, the CDC will enumerate and appear as
/dev/ttyACM#
.
On MAC machines, the CDC will enumerate and appear as
/dev/tty.usbmodem#
. Depending on which terminal program is used, it
will appear in the available list of modems as usbmodem#
.