The Log window displays the following:
- Informational messages such as the location and name of the files used to display
the view.
- Any syntax errors in the HDL file if
the HDL file is opened with the Open File Location option (right-click design
object > Open File Location).
Note: The Log window displays by
default when the Netlist Viewer opens. Hiding the Log window will leave more display area
for the Canvas view. To get a larger display area for the Canvas view, hide the Log window
(
Netlist Viewer >
Windows and
uncheck
Show Log)
Figure 1. Log Window