The status bar at the bottom-right corner of the Netlist Viewer displays
the following:
- Mode — displays Global or Local mode.
Global mode means the Netlist Viewer can cross hierarchical boundaries when following
nets to drivers or loads. Local means the Netlist Viewer stays in the current level
of design hierarchy.
- Current Level — displays the current
level of design hierarchy, either TOP_LEVEL instance name or instance name of the
component.
- Current Page — displays the current
page of the Netlist Viewer (Page x of <total>) when traversing across different
pages of the Netlist Viewer.
- Fam — displays the technology
family.
Figure 1. Status Bar