Running the Example
- Connect the keypad to the ATmega1627
Curiosity Nano as follows:
- Row 0: PB0
- Row 1: PB1
- Row 2: PA2
- Row 3: PA1
- Column 0: PC3
- Column 1: PC0
- Column 2: PC1
- Column 3: PC2
- Connect the red LED to PB3 and the green LED to PB2
- Connect the ATtiny1627 Curiosity Nano
to a computer using a USB cable
- Download the application as explained
in Section Get Code Examples from Atmel START and program it to the ATtiny1627 Curiosity Nano
- The pin code “123ABC” is programmed
to be the passcode. Try pressing this code followed by pound (#) to observe the
green LED flashing. Try a different code to observe the red LED flashing.