The following instructions show how to analyze power consumption using the Power Debugger
and Data Visualizer.
Power Debugger connection:
- 1.Connect one of the ground
reference pins of the Power Debugger to a ground pin on the Curiosity Nano
board.
- 2.Connect the VOFF pin on the
Curiosity Nano board to a ground pin to turn off the connection between the USB
power supply and the tinyAVR device.
- 3.Connect the VBUS pin on the
Curiosity Nano board to the the input current pin of measurement circuit A on
the Power Debugger.
- 4.Connect the output current pin of
measurement circuit A on the Power Debugger to the VTG pin on the Curiosity Nano
board.
Measurement circuit A of the Power Debugger is now connected in series between the
USB voltage source and the tinyAVR microcontroller, and can measure the total current
used.
Figure 1. Power Debugger Connection
Data Visualizer setup:
- 1.Open Data
Visualizer.
- 2.Open in Data Visualizer.
- 3.On the DGI Control
Panel pane, select .
- 4.Check the
Power check box.
- 5.Expand the Channel
A dropdown in the Control Panel in the
Power Analysis pane.
- 6.Drag the plug from A
Current in the DGI Control Panel pane to
the Current socket in the Power
Analysis pane.
- 7.Press Start in the DGI Control
Panel pane.
- 8.Optional: Enable cursors by
checking the Enabled check box in the
Cursors dropdown.
Figure 2. Power Debugging Graph in Data Visualizer