The Port C pins with alternate functions are shown in the table below:
Port Pin | Alternate Function |
---|---|
PC6 | RESET (Reset pin) |
PC5 | ADC5 (ADC
Input Channel 5) SCL (Two-wire Serial Bus Clock Line) |
PC4 | ADC4 (ADC
Input Channel 4) SDA (Two-wire Serial Bus Data Input/Output Line) |
PC3 | ADC3 (ADC Input Channel 3) |
PC2 | ADC2 (ADC Input Channel 2) |
PC1 | ADC1 (ADC Input Channel 1) |
PC0 | ADC0 (ADC Input Channel 0) |
The alternate pin configuration is as follows:
• RESET – Port C, Bit 6
RESET, Reset pin: When the RSTDISBL Fuse is programmed, this pin functions as a normal I/O pin, and the part will have to rely on Power-on Reset and Brown-out Reset as its reset sources. When the RSTDISBL Fuse is unprogrammed, the reset circuitry is connected to the pin, and the pin can not be used as an I/O pin.
If PC6 is used as a reset pin, DDC6, PORTC6 and PINC6 will all read 0.
• SCL/ADC5 – Port C, Bit 5
SCL, Two-wire Serial Interface Clock: When the TWEN bit in TWCR is set (one) to enable the Two-wire Serial Interface, pin PC5 is disconnected from the port and becomes the Serial Clock I/O pin for the Two-wire Serial Interface. In this mode, there is a spike filter on the pin to suppress spikes shorter than 50 ns on the input signal, and the pin is driven by an open drain driver with slew-rate limitation.
PC5 can also be used as ADC input Channel 5. Note that ADC input channel 5 uses digital power.
• SDA/ADC4 – Port C, Bit 4
SDA, Two-wire Serial Interface Data: When the TWEN bit in TWCR is set (one) to enable the Two-wire Serial Interface, pin PC4 is disconnected from the port and becomes the Serial Data I/O pin for the Two-wire Serial Interface. In this mode, there is a spike filter on the pin to suppress spikes shorter than 50 ns on the input signal, and the pin is driven by an open drain driver with slew-rate limitation.
PC4 can also be used as ADC input Channel 4. Note that ADC input channel 4 uses digital power.
• ADC3 – Port C, Bit 3
PC3 can also be used as ADC input Channel 3. Note that ADC input channel 3 uses analog power.
• ADC2 – Port C, Bit 2
PC2 can also be used as ADC input Channel 2. Note that ADC input channel 2 uses analog power.
• ADC1 – Port C, Bit 1
PC1 can also be used as ADC input Channel 1. Note that ADC input channel 1 uses analog power.
• ADC0 – Port C, Bit 0
PC0 can also be used as ADC input Channel 0. Note that ADC input channel 0 uses analog power.
The tables below relate the alternate functions of Port C to the overriding signals shown in figure Figure 1.
Signal Name | PC6/RESET | PC5/SCL/ADC5 | PC4/SDA/ADC4 |
---|---|---|---|
PUOE | RSTDISBL | TWEN | TWEN |
PUOV | 1 | PORTC5 • PUD | PORTC4 • PUD |
DDOE | RSTDISBL | TWEN | TWEN |
DDOV | 0 | SCL_OUT | SDA_OUT |
PVOE | 0 | TWEN | TWEN |
PVOV | 0 | 0 | 0 |
DIEOE | RSTDISBL | 0 | 0 |
DIEOV | 0 | 0 | 0 |
DI | – | – | – |
AIO | RESET INPUT | ADC5 INPUT / SCL INPUT | ADC4 INPUT / SDA INPUT |
Signal Name | PC3/A11 | PC2/A10 | PC1/A9 | PC0/A8 |
---|---|---|---|---|
PUOE | 0 | 0 | 0 | 0 |
PUOV | 0 | 0 | 0 | 0 |
DDOE | 0 | 0 | 0 | 0 |
DDOV | 0 | 0 | 0 | 0 |
PVOE | 0 | 0 | 0 | 0 |
PVOV | 0 | 0 | 0 | 0 |
DIEOE | 0 | 0 | 0 | 0 |
DIEOV | 0 | 0 | 0 | 0 |
DI | – | – | – | – |
AIO | ADC3 INPUT | ADC2 INPUT | ADC1 INPUT | ADC0 INPUT |