The Receiver buffer FIFO will be flushed when the Receiver is disabled (i.e., the buffer will be emptied of its contents). Unread data will be lost. If the buffer has to be flushed during normal operation, due to for instance an error condition, read the UDR I/O location until the RXC Flag is cleared. The following code example shows how to flush the receive buffer.
USART_Flush: sbis r16, RXC ret in r16, UDR rjmp USART_Flush
void USART_Flush( void ) { unsigned char dummy; while ( UCSRA & (1<<RXC) ) dummy = UDR; }