8-bit AVR Microcontroller

Interrupt Vectors in ATmega8A

Table 1. Reset and Interrupt Vectors
Vector No. Program
Address(2) Source Interrupt Definition
1 0x000(1) RESET External Pin, Power-on Reset, Brown-out Reset, and Watchdog Reset
2 0x001 INT0 External Interrupt Request 0
3 0x002 INT1 External Interrupt Request 1
4 0x003 TIMER2 COMP Timer/Counter2 Compare Match
5 0x004 TIMER2 OVF Timer/Counter2 Overflow
6 0x005 TIMER1 CAPT Timer/Counter1 Capture Event
7 0x006 TIMER1 COMPA Timer/Counter1 Compare Match A
8 0x007 TIMER1 COMPB Timer/Counter1 Compare Match B
9 0x008 TIMER1 OVF Timer/Counter1 Overflow
10 0x009 TIMER0 OVF Timer/Counter0 Overflow
11 0x00A SPI, STC Serial Transfer Complete
12 0x00B USART, RXC USART, Rx Complete
13 0x00C USART, UDRE USART Data Register Empty
14 0x00D USART, TXC USART, Tx Complete
15 0x00E ADC ADC Conversion Complete
16 0x00F EE_RDY EEPROM Ready
17 0x010 ANA_COMP Analog Comparator
18 0x011 TWI Two-wire Serial Interface
19 0x012 SPM_RDY Store Program Memory Ready
Notes:
  1. 1.When the BOOTRST Fuse is programmed, the device will jump to the Boot Loader address at reset, see Boot Loader Support – Read-While-Write Self-Programming.
  2. 2.When the IVSEL bit in GICR is set, Interrupt Vectors will be moved to the start of the boot Flash section. The address of each Interrupt Vector will then be the address in this table added to the start address of the boot Flash section.

The next table shows reset and Interrupt Vectors placement for the various combinations of BOOTRST and IVSEL settings. If the program never enables an interrupt source, the Interrupt Vectors are not used, and regular program code can be placed at these locations. This is also the case if the Reset Vector is in the Application section while the Interrupt Vectors are in the boot section or vice versa.

Table 2. Reset and Interrupt Vectors Placement
BOOTRST(1) IVSEL Reset Address Interrupt Vectors Start Address
1 0 0x000 0x001
1 1 0x000 Boot Reset Address + 0x001
0 0 Boot Reset Address 0x001
0 1 Boot Reset Address Boot Reset Address + 0x001
Note: 1. The Boot Reset Address is shown in table Boot Size Configuration in the Boot Loader Parameters section. For the BOOTRST Fuse “1” means unprogrammed while “0” means programmed.

The most typical and general program setup for the Reset and Interrupt Vector Addresses in ATmega8A is:

address Labels Code   Comments
$000   rjmp RESET ; Reset Handler
$001   rjmp EXT_INT0 ; IRQ0 Handler
$002   rjmp EXT_INT1 ; IRQ1 Handler
$003   rjmp TIM2_COMP ; Timer2 Compare Handler
$004   rjmp TIM2_OVF ; Timer2 Overflow Handler
$005   rjmp TIM1_CAPT ; Timer1 Capture Handler
$006   rjmp TIM1_COMPA ; Timer1 CompareA Handler
$007   rjmp TIM1_COMPB ; Timer1 CompareB Handler
$008   rjmp TIM1_OVF ; Timer1 Overflow Handler
$009   rjmp TIM0_OVF ; Timer0 Overflow Handler
$00a   rjmp SPI_STC ; SPI Transfer Complete Handler
$00b   rjmp USART_RXC ; USART RX Complete Handler
$00c   rjmp USART_UDRE ; UDR Empty Handler
$00d   rjmp USART_TXC ; USART TX Complete Handler
$00e   rjmp ADC ; ADC Conversion Complete Handler
$00f   rjmp EE_RDY ; EEPROM Ready Handler
$010   rjmp ANA_COMP ; Analog Comparator Handler
$011   rjmp TWSI ; Two-wire Serial Interface Handler
$012   rjmp SPM_RDY ; Store Program Memory Ready Handler
;        
$013 RESET: ldi r16,high(RAMEND) ; Main program start
$014   out SPH,r16$013 ; Set Stack Pointer to top of RAM
$015   ldi r16,low(RAMEND)$013  
$016   out SPL,r16$013  
$017   sei   ; Enable interrupts
$018   <instr> XXX  
:.   :. :.  

When the BOOTRST Fuse is unprogrammed, the boot section size set to 2K bytes and the IVSEL bit in the GICR Register is set before any interrupts are enabled, the most typical and general program setup for the Reset and Interrupt Vector Addresses is:

Adddress Labels Code Comments
$000 rjmp RESET ; Reset handler
;
$001 RESET: ldi r16,high(RAMEND) ; Main program start
$002 out SPH,r16 ; Set Stack Pointer to top of RAM
$003 ldi r16,low(RAMEND)
$004 out SPL,r16
$005 sei ; Enable interrupts
$006 <instr> XXX
;
.org $c01
$c01 rjmp EXT_INT0 ; IRQ Handler
$c02 rjmp EXT_INT1 ; IRQ| Handler
:. :. :.
$c12 rjmp SPM_RDY ; Store Program Memory Ready Handler

When the BOOTRST Fuse is programmed and the boot section size set to 2K bytes, the most typical and general program setup for the Reset and Interrupt Vector Addresses is:

Address Labels Code   Comments
.org $001        
$001   rjmp EXT_INT0 ; IRQ0 Handler
$002     EXT_INT1 ; IRQ1 Handler
:.   :. :. ;
$012   rjmp SPM_RDY ; Store Program Memory Handler
;        
.org $c00        
$c00   rjmp RESET ; Reset handler
;        
$c01 RESET: ldi r16,high(RAMEND) ; Main program start
$c02   out SPH,r16 ; Set Stack Pointer to top of RAM
$c03   ldi r16,low(RAMENSPL,r16D)  
$c04   out SPL,r16  
$c05   sei   ; Enable interrupts
$c06   <instr> XXX  

When the BOOTRST Fuse is programmed, the boot section size set to 2K bytes, and the IVSEL bit in the GICR Register is set before any interrupts are enabled, the most typical and general program setup for the Reset and Interrupt Vector Addresses is:

Address Labels Code   Comments
;        
.org $c00        
$c00   rjmp RESET ; Reset handler
$c01   rjmp EXT_INT0 ; IRQ0 Handler
$c02   rjmp EXT_INT1 ; IRQ1 Handler
:.   :. :.  
$c12   rjmp SPM_RDY ; Store Program Memory Ready Handler
$c13 RESET: ldi r16,high(RAMEND) ; Main program start
$c14   out SPH,r16 ; Set Stack Pointer to top of RAM
$c15   ldi r16,low(RAMEND)  
$c16   out SPL,r16  
$c17   sei   ; Enable interrupts
$c18   <instr> XXX