The operational range of the Receiver is dependent on the mismatch between the received bit rate and the internally generated baud rate. If the Transmitter is sending frames at too fast or too slow bit rates, or the internally generated baud rate of the Receiver does not have a similar (refer to next table) base frequency, the Receiver will not be able to synchronize the frames to the start bit.
The following equations can be used to calculate the ratio of the incoming data rate and internal receiver baud rate.
First sample number used for majority voting. SF = 8 for Normal Speed and SF = 4 for Double Speed mode. | |
The following tables list the maximum receiver baud rate error that can be tolerated. Note that Normal Speed mode has higher toleration of baud rate variations.
D # (Data+Parity Bit) | Rslow [%] | Rfast [%] | Max. Total Error [%] | Recommended Max Receiver Error [%] |
---|---|---|---|---|
5 | 93.20 | 106.67 | +6.67/-6.8 | ±3.0 |
6 | 94.12 | 105.79 | +5.79/-5.88 | ±2.5 |
7 | 94.81 | 105.11 | +5.11/-5.19 | ±2.0 |
8 | 95.36 | 104.58 | +4.58/-4.54 | ±2.0 |
9 | 95.81 | 104.14 | +4.14/-4.19 | ±1.5 |
10 | 96.17 | 103.78 | +3.78/-3.83 | ±1.5 |
D # (Data+Parity Bit) | Rslow [%] | Rfast [%] | Max Total Error [%] | Recommended Max Receiver Error [%] |
---|---|---|---|---|
5 | 94.12 | 105.66 | +5.66/-5.88 | ±2.5 |
6 | 94.92 | 104.92 | +4.92/-5.08 | ±2.0 |
7 | 95.52 | 104.35 | +4.35/-4.48 | ±1.5 |
8 | 96.00 | 103.90 | +3.90/-4.00 | ±1.5 |
9 | 96.39 | 103.53 | +3.53/-3.61 | ±1.5 |
10 | 96.70 | 103.23 | +3.23/-3.30 | ±1.0 |
The recommendations of the maximum Receiver baud rate error was made under the assumption that the Receiver and Transmitter equally divides the maximum total error.
There are two possible sources for the Receivers Baud Rate error. The Receiver’s system clock (XTAL) will always have some minor instability over the supply voltage range and the temperature range. When using a crystal to generate the system clock, this is rarely a problem, but for a resonator the system clock may differ more than 2% depending of the resonators tolerance. The second source for the error is more controllable. The baud rate generator can not always do an exact division of the system frequency to get the baud rate wanted. In this case an UBRR value that gives an acceptable low error can be used if possible.