The following recommendations must be applied for the placement of the antenna and its
cable:
- The antenna cable must not be routed over circuits generating electrical noise on
the host board or alongside or underneath the module. It is preferred that the cable
be routed straight out of the module.
- The antenna must not be placed in direct contact or in close proximity of the
plastic casing/objects.
- Do not enclose the antenna within a metal shield.
- Keep any components which may radiate noise, signals or harmonics within the 2.4 GHz
to 2.5 GHz frequency band away from the antenna and, if possible, shield those
components. Any noise radiated from the host board in this frequency band degrades
the sensitivity of the module.
- The antenna should preferably be placed at a distance greater than 5 cm away from
the module. The following figure shows the antenna keep-out area indication; where
the antenna must not be placed in this area. This recommendation is based on an
open-air measurement and does not take into account any metal shielding of the
customer end product. When a metal enclosure is used, the antenna can be located
closer to the ATWINC15x0-MR210UB module.
The drawing below provides an indication of how the antenna cable should be routed
depending on the location of the antenna with respect to the ATWINC15x0-MR210UB PCB. There are two possible options for the optimum routing
of the cable.
Figure 1. ATWINC15x0-MR210UB Antenna Placement
Guidelines
Note: These are generic guidelines and it is recommended that customers check and fine-tune
the antenna positioning in the final host product based on RF performance.