The Program Flash Memory and User ID are programmed one word at a time. The EEPROM memory
and configuration regions are programmed one byte at a time.
Figure 1. Device Program/Verify
Flowchart
Figure 2. Program Memory Flowchart
Notes:
- 1.This step is optional if the
device has already been erased or has not been previously programmed.
- 2.If the device is code-protected
or must be completely erased, then Bulk Erase the device, as shown in Figure 5.
Figure 3. One-Word Program Cycle
Figure 4. User ID and Configuration Memory
Program Flowchart
Notes:
- 1.This step is optional if the
device has already been erased or has not been previously programmed.
- 2.See Figure 3.
Figure 5. Bulk Erase Flowchart