Once a device has entered the ICSP Program/Verify mode (using either high-voltage or LVP entry), the programming host device may issue six commands to the microcontroller, each eight bits in length. The commands are summarized in Table 1 and are used to erase or program the device based on the location of the Program Counter (PC).
Some 8-bit commands also have an associated data payload (such as Load PC Address and Read Data from NVM).
If the host device issues an 8-bit command byte that has an associated data payload, the host device is responsible for sending additional 24 clock pulses (e.g., three 8-bit bytes) to send or receive the payload data associated with the command.
The payload field size is compatible with many 8-bit SPI-based systems. Within each 24-bit payload field, the first bit transmitted is always a Start bit, followed by a variable number of Pad bits, then by the useful data payload bits and ending with one Stop bit. The useful data payload bits are always transmitted MSb first.
When the programming device issues a command that involves a host to the microcontroller
payload (e.g., Load PC Address), the Start, Stop and Pad bits will all be driven by the
programmer to ‘0
’. When the programming host device issues a command
that involves the microcontroller to host payload data (e.g., Read Data from NVM), the
Start, Stop and Pad bits will be treated as ‘don't care’ bits and the values will be
ignored by the host.
When the programming host device issues an 8-bit command byte to the microcontroller, the host will wait a specified minimum amount of delay (which is command-specific) prior to sending any additional clock pulses (associated with either a 24-bit data payload field or the next command byte).
Command Name | Command Value | Payload Expected | Delay after Command | Data/Note | |
---|---|---|---|---|---|
Binary (MSb … LSb) | Hex | ||||
Load PC Address | 1000 0000 |
80 | Yes | TDLY | Payload value = PC |
Bulk Erase | 0001 1000 |
18 | Yes | TERAB | The payload carries the information of the regions that need to be bulk erased |
Page Erase Program Memory | 1111 0000 |
F0 | No | TERAS | The page addressed by the MSbs of the PC is erased; LSbs are ignored |
Read Data from NVM | 1111 11J0 |
FC/FE | Yes | TDLY | Data output ‘0 ’ if code-protect is
enabled:
J = J = |
Increment Address | 1111 1000 |
F8 | No | TDLY | PC = PC + n(2) |
Program Data | 11J0 0000 |
C0/E0 | Yes | TPROG | Payload value = Data
Word; J = J = |