Running the Example
- 1.Connect the modified Click board to
slot 3 of the Curiosity Nano Base for Click boards™.
- 2.Connect the ATtiny1627 Curiosity Nano
to the Curiosity Nano Base for Click boards™.
- 3.Connect the ATtiny1627 Curiosity Nano
to a computer using a USB cable.
- 4.Download the application, as
explained in Section Get Code Examples from Atmel START or Section Get Code Examples from GitHub.
- 5.Choose one of the two code projects
and program the ATtiny1627.
- 6.Wave a hand or walk in front of the
sensor and observe the red LED flashing.