To read the contents of the WPR, a random read operation must be sent to the device (see Random Read) so that the reserved word address bits A7 and A6 can properly be set. It is not possible to read the contents of the WPR with a current address read.
0
’ as seen in Table 3.For the AT24CSW04X, the @ indicates the A1 address bit which is managed by the ordering code of the device (see Table 3). For the AT24CSW08X, the @ indicates the A9 address bit.