Join Procedure

This section captures the power profile during the joining process with the network server, and also highlights the profile on the following modes:

The following table provides the settings for profiling the join procedure.

Table 1. Settings for Profiling the Join Procedure

Attribute

Value

TX data rate

DR0 and DR5

RX1 data rate

Same as TX data rate

RX2 data rate

DR0

Join accept delay 1

5s

Join accept delay 2

6s

TX power(1)

1 (default)

Note:
  1. 1.The TX power from the preceding table resembles the offset value from the TX power table as per the RP2-1.0.2 LoRaWAN® Regional Parameters. Calculate the equivalent TX power value at the radio level for the above offset value using the following equation:
    Figure 1. Equivalent TX Power
    EquivalentTXPower=MAXEIRP2dB=162=14dBm
    • Join accept delay 1 is the delay between the TX state and RX1 state
    • Join accept delay 2 is the delay between the TX state and RX2 state

The following plots illustrate the transmission of the join request, reception of the join accept in the RX1 window and reception of the join accept in the RX2 at transmission data rates DR0 and DR5 followed by their respective zoomed-in plots with consumption values in each state.

Figure 2. Join Request Transmission and Join Accept in RX1 Event “With Period of Operation” at DR0


Figure 3. Join Request Transmission and Join Accept in RX1 Event “With Period of Operation” at DR5


Figure 4. Join Request Transmission “With Period of Operation” Zoom in Plot at DR0


Figure 5. Join Request Transmission “With Period of Operation” Zoom in Plot at DR5


Figure 6. Join Accept Reception in RX1 “With Period of Operation” Zoom in Plot at DR0


Figure 7. Join Accept Reception in RX1 “With Period of Operation” Zoom in Plot at DR5


Figure 8. Join Accept Delay 1 “With Period of Operation” Zoom in Plot at DR0


Figure 9. Join Accept Delay 1 “With Period of Operation” Zoom in Plot at DR5


Figure 10. Join Request Transmission and Reception of Join Accept in RX2 “With Period Of Operation” at DR0


Figure 11. Join Request Transmission and Reception of Join Accept In RX2 “With Period Of Operation” at DR5


Figure 12. Receive Window 1 Open Event “With Period of Operation” Zoom in Plot at DR0


Figure 13. Receive Window 1 Open Event “With Period of Operation” Zoom in Plot at DR5


Figure 14. Join Accept Delay 2 Event “With Period of Operation” Zoom in Plot at DR0


Figure 15. Join Accept Delay 2 Event “With Period of Operation” Zoom in Plot at DR5


Figure 16. Join Accept Reception in RX2 “With Period of Operation” Zoom in Plot at DR0


Figure 17. Join Accept Reception in RX2 “With Period of Operation” Zoom in Plot at DR5


Figure 18. Join Request Transmission and Join Accept in RX1 Event “Without Period of Operation” at DR0


Figure 19. Join Request Transmission and Join Accept in RX1 Event “Without Period of Operation” at DR5


Figure 20. Join Request Transmission “Without Period of Operation” Zoom in Plot at DR0


Figure 21. Join Request Transmission “Without Period of Operation” Zoom in Plot at DR5


Figure 22. Join Accept Reception in RX1 “Without Period of Operation” Zoom in Plot at DR0


Figure 23. Join Accept Reception in RX1 “Without Period of Operation” Zoom in Plot at DR5


Figure 24. Join Accept Delay 1 “Without Period of Operation” Zoom in Plot at DR0


Figure 25. Join Accept Delay 1 “Without Period of Operation” Zoom in Plot at DR5


Figure 26. Join Request Transmission and Reception of Join Accept in RX2 “Without Period of Operation” at DR0


Figure 27. Join Request Transmission & Reception of Join Accept in RX2 “Without Period of Operation” DR5


Figure 28. Receive Window 1 Open Event “Without Period of Operation” Zoom in Plot at DR0


Figure 29. Receive Window 1 Open Event “Without Period of Operation” Zoom in Plot at DR5


Figure 30. Join Accept Delay 2 Event “Without Period of Operation” Zoom in Plot at DR0


Figure 31. Join Accept Delay 2 Event “Without Period of Operation” Zoom in Plot at DR5


Figure 32. Join Accept Reception in RX2 “Without Period of Operation” Zoom in Plot at DR0


Figure 33. Join Accept Reception in RX2 “Without Period of Operation” Zoom in Plot at DR5


From the preceding plots, the total time taken to complete the transaction at different data rate scenarios is given in the following table.

Table 2. Total Time Taken to Complete the Transaction

Data Rate

Total Time Taken to Complete the Transaction

Units

Join Request Transmission and Join Accept in RX1 (Transaction Event 1)

Join Request Transmission and Join Accept in RX2 (Transaction Event 2)

DR0

8.33

9.35

seconds

DR5

5.15

7.90

seconds
Notes: The MAC state sequence (inside MLS) during transaction event 1 and transaction event 2 are as follows:
Table 3. Join Request Transmission Event (TX) – MAC STATE: TX_OCCURING
Attribute Measured Value Units
DR0 DR5

Total duration

1484

68.70

ms

Average current

34.81

32.02

mA

Peak current

37.80

38.02

mA

Total charge

51658.04

2199.78

mA×ms
Table 4. Join Accept Delay 1 – MAC STATE: BEFORE_RX1

Attribute

Measured Value

Units

DR0

DR5

Total duration

4973

4937

ms

Average current

1.487

1.548

mA

Peak current

1.638

1.621

mA

Total charge

7394.86

7642.48

mA×ms
Table 5. Join Accept Reception in RX1 Receive Window – MAC STATE: RX1_OPEN

Attribute

Measured Value

Units

DR0

DR5

Total duration (ms)

1878

134.2

ms

Average current (mA)

13.84

13.41

mA

Peak current (mA)

14.82

15.25

mA

Total charge (mA×ms)

25991.52

1799.63

mA×ms
Table 6. Join Accept Delay 2 – MAC STATE: BETWEEN_RX1_RX2

Attribute

Measured Value

Units

DR0

DR5

Total duration

717.9

949

ms

Average current

1.440

1.490

mA

Peak current

1.564

1.641

mA

Total charge

1033.78

1414.01

mA×ms
Table 7. Join Accept Reception in RX2 Receive Window – MAC STATE: RX2_OPEN

Attribute

Measured Value

Units

DR0

DR5

Total duration

1862

1862

ms

Average current

13.98

13.3

mA

Peak current

16.21

17.05

mA

Total charge

26030.8

24764.6

mA×ms
Table 8. Receive Window 1 Open When Reception of Join Accept in RX2 Window – MAC STATE: RX1_OPEN

Attribute

Measured Value

Units

DR0

DR5

Total duration

265.5

87.61

ms

Average current

13.87

13.55

mA

Peak current

15.21

17.40

mA

Total charge

3682.5

1187.12

mA×ms

The following table provides the time stamp reference for each join request sent and join accept received in RX1 and RX2 reception windows.

Note: Initiate multiple join requests to capture the reception of the join accept frame in each of the receive windows (RX1 and RX2). Disable the join accept 1 (RX1) window on the network server side to receive the join accept packet in the RX2 receive window in the WLR089 device.
Table 9. Join Request and Join Accept in RX1 Snippet

Packet N

Packet Type

Time Stamp

Source

Destination

DR0

DR5

Packet 1

Join request 1

12:56:23.457

12:34:43.860

End device (WLR089)

Network server

Packet 2

Join accept in RX1

12:56:32.788

12:34:49.005

Network server

End device (WLR089) – RX1

Table 10. Join Request and Join Accept in RX2 Snippet

Packet N

Packet Type

Time Stamp

Source

Destination

DR0

DR5

Packet 1

Join request 2

12:57:53.677

12:37:04.189

End device (WLR089)

Network server

Packet 2

Join accept in RX2

12:57:03.002

12:37:12.095

Network server

End device (WLR089) – RX2