This application note describes the power consumption profile of the WLR089 device under various application scenarios in Long
Range (LoRa®) technology. The profiling of the WLR089 device captures various
application scenarios based on the following connection types:
- Long Range Wide Area Network
(LoRaWAN) (Node <-> Gateway <-> Network Server)
- Initialization
- Join Procedure
- Uplink Data Transmission
- Downlink Data Reception
- Sleep Mode Operation
- Persistent Data Server (PDS) Operation
- LoRa Modulation (Node to Node)
- Data Transmission
- Data Reception
This application note:
- Helps the user to estimate the
expected power consumption in the WLR089 device
based on their tailored application needs
- Details the setup to perform the
power measurements using the WLR089 Xplained Pro Evaluation board. This is also a reference to estimate the power
consumption with the custom board (using the WLR089 device) in real life applications.
- Briefs the configurable
parameters in both the LoRa connection type and the LoRaWAN connection type. The
user can fine tune these configurable parameters to optimize further.
Figure 1. WLR089 Xplained Pro Evaluation Kit
Note: This application note captures
the measurement results from a random sample. The reported values are only for
estimation. The actual value may vary from device to device.