When dropping the application firmware, build the application with ROM region starting
address set at 0x10000. If the ROM Starting address is not set properly, then the
programming will not work correctly.
Select the starting application address in H3 to 0x10000 in the “system” component as
follows: