In Full Bridge mode, changing the MODE[0] bit controls the forward/reverse direction. Direction changes occur
on the next rising edge of the modulated input. The sequence, described as follows, is
illustrated in Figure 1.
- 1.The associated active output CWGxA and the inactive output CWGxC are switched to
drive in the opposite direction.
- 2.The previously modulated output CWGxD is switched to the Inactive state, and the
previously inactive output CWGxB begins to modulate.
- 3.CWG modulation resumes after the direction-switch dead band has elapsed.
Figure 1. Example of PWM Direction Change at
Near 100% Duty Cycle