The unlock sequence is a mechanism that protects the DFM from unintended self-write programming or erasing. The sequence must be executed and completed without interruption to successfully complete an erase or write operation.
The unlock sequence consists of the following steps and must be completed in order:
Once the WR bit is set, the processor will stall internal operations until the operation is complete and then resume with the next instruction.
Since the unlock sequence must not be interrupted, global interrupts must be disabled prior to the unlock sequence and re-enabled after the unlock sequence is completed.
NVMCON1bits.WREN = 1; // Enable write/erase
INTCONbits.GIE = 0; // Disable global interrupts
// The next three steps are the required unlock sequence
NVMCON2 = 0x55; // First unlock code
NVMCON2 = 0xAA; // Second unlock code
NVMCON1bits.WR = 1; // Initiate write/erase cycle
INTCONbits.GIE = 1; // Enable global interrupts
NVMCON1bits.WREN = 0; // Disable further write/erase cycles