Power and Ground
- Dedicate the layer immediately
below the layer containing the RF traces from the ATWINC15x0B for the ground. Ensure that this ground plane does not get
broken up by routes.
- Power traces can be routed on all layers except the ground layer.
- Power supply routes must be heavy
copper fill planes to ensure low inductance.
- The power pins of the ATWINC15x0B must have a via directly to the power
plane, close to the power pin.
- Decoupling capacitors must have a
via next to the capacitor pin and this via must be directly connected to the
power plane and avoid a long trace for this connection.
- The ground pad of the decoupling
capacitor must have a via directly connected to the ground plane.
- Each decoupling capacitor must
have its own via directly connected to the ground plane and directly connected
to the power plane next to the pad.
- The decoupling capacitors must be placed as close as possible to the pin that it
is filtering.