The AVR64DD32 Curiosity Nano board has one mechanical switch - a
generic user-configurable switch. Pressing the switch will drive the I/O line to ground
(GND).
Tip: There is no externally
connected pull-up resistor on the switch. Be sure that an internal pull-up resistor is
enabled on pin PF6 to use the
switch.