No software configuration is required to program and debug the same device mounted on the
board.
To program and debug a different microcontroller than what is mounted on the board,
Microchip Studio must be configured to allow a free selection of devices and programming
interfaces.
- 1.Navigate to through the menu system at the top of the application.
- 2.Select the category in the options window.
- 3.Set the Hide unsupported
devices option to False.
Figure 1. Hide Unsupported Devices
Info:
Microchip Studio allows any microcontroller and interface to be selected when the
Hide unsupported devices setting is set to False - also
microcontrollers and interfaces not supported by the on-board debugger.