On Windows® machines, the CDC will enumerate as Curiosity Virtual COM Port and appear in the Ports section of the Windows Device Manager. The COM port number can also be found there.
On Linux® machines, the CDC will enumerate and appear as
/dev/ttyACM#
.
On Mac® machines, the CDC will enumerate and appear as
/dev/tty.usbmodem#
. Depending on the terminal program used, it will
appear in the available list of modems as usbmodem#
.