In the Key Config mode of the GenDig
command,
the slot configuration and key configuration of the key specified by
KeyID are included in the GenDig TempKey calculation. The
Nonce
command must be run prior to the first
GenDig
command to load a value into TempKey.
Subsequent GenDig
commands will use the value from
the previous GenDig operation.
Opcode |
Mode |
KeyID(1) |
Data |
Description |
---|---|---|---|---|
0x15 | 0x05 | 0x00 0[Slot] | — | Includes slot configuration information |
Name | Size | Description |
---|---|---|
Response | 1 byte |
0x00 - If successful. Error code - If the command fails. |
32 bytes |
TempKey.value |