Data from the Data zone slots can be included in the GenDig calculation. Data
are always included in 32-byte blocks and only the lowest block of a slot is included in
the GenDig calculation. The Nonce
command must be run prior to the
first GenDig
command to load a value into TempKey. If the slot requires
a random nonce, then the data must be generated by the Nonce
command
versus passing it into the device. Subsequent GenDig
commands will use
the value from the previous GenDig operation.
If a slot is set for NoMAC, then it is not allowed to use the output of this
GenDig in a MAC
command. If multiple GenDigs are run, if any slot has
NoMAC set, then the output in TempKey cannot be used in executing a MAC
command.
Opcode |
Mode |
KeyID(1) |
Data |
Description |
---|---|---|---|---|
0x15 | 0x02 | 0x00 0[Slot] | — | Use data from slot # in the calculation. |
0x00 0[Slot] | 4 bytes | Use data from slot # in the calculation and other data when using a NoMAC key slot |
Name | Size | Description |
---|---|---|
Response | 1 byte |
0x00 - If successful. Error code - If the command fails. |
MAC
command is allowed and 1 if it is not.Size | Parameters - MAC | Parameters - NoMAC |
---|---|---|
32 bytes | DATA.slot[KeyID] | DATA.slot[KeyID] |
4 byte | Opcode, Mode, KeyID = 0x15, 0x02, 0x0[Slot] 0x00 | OtherData[0:3] |
1 byte | SN[8] = Varies by vendor | SN[8] = Varies by vendor |
2 bytes | SN[0:1] = 0x01 0x23 | SN[0:1] = 0x01 0x23 |
25 bytes | All Zeros | All Zeros |
32 bytes | TempKey.Value | TempKey.Value |